Dears,
I tried to build project "MCSPTE1AK144_BLDC_6Step" in order to get file for flashing of MCU (MCSPTE1AK144_BLDC_6Step.srec) in version MCSPTE1AK144 Development Kit Application Software 1.2.
In difference from version 1.1 I got in this build in ver.1.2 the error message (pls see attached file Error Message.jpg). The S32DS extension and updates is on attached picture 240311 S32 Desig StudioCapture.jpg. See also note bellow [1].
Before work I set parameetrs for LINIX motor by running SetMotor-LINIX_45ZWN24-40.bat.
As I wrote - the build in version 1.1 is without problem.
Thank you very much for your kindly help
Juraj, teacher & development eng in Schaeffler AG.
[1]
- S32 Design Studio (S32DS) for ARM 2.2
- S32 Software Development Kit (SDK) for S32K1xx 3.0.3
- S32K14x_AMMCLIB_v1.1.35
- FreeMASTER 3.1.4.5
已解决! 转到解答。
Hello,
It looks you are missing gdflib.h
This is part of AMMCLIB. Set your library paths accordingly your files location in project settings.
Includes and also libraries paths.
Best regards,
Peter
Hello,
It looks you are missing gdflib.h
This is part of AMMCLIB. Set your library paths accordingly your files location in project settings.
Includes and also libraries paths.
Best regards,
Peter
Hi Peter,
thank you very much for your reply. I'll try do it.
I want remark that project mentioned by my is a part of delivery of SW for EvaKit from NXP ver.1.2. and in such way it should not contains such errors ( as a sample it should be "buildable " without additional effort). The ver 1.1 of SW for this EvaKIt is OK - this ver.1.2 need additional efort as you wrote.
Thank again. Have a nice day. Juraj