LPIT Chanuel Re-Init Issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPIT Chanuel Re-Init Issue

1,106 次查看
赵子成
Contributor IV

Hi All,

My software contains BOOT and APP, LPIT CHANNEL1 is used in both BOOT and APP. If I don't stop the LPIT channel before jumpping to APP from BOOT via "LPIT_DRV_StopTimerChannels(INST_LPIT1, (1 << LPIT_CHANNEL1))", in the APP Init phase, in LPIT Init, when exec the init function "LPIT_DRV_InitChannel(INST_LPIT1, LPIT_CHANNEL1, &lpit1_ChnConfig1);", will lead to DefaultISR, I don't know why, Can someone answer my issue? Thanks.

I use LPIT timer interrupt function both in BOOT and APP.

The BOOT and APP is run in PFLASH, and they have own INT VEC.

The BOOT LPIT Init code:

void LPIT_Init(void)
{
LPIT_DRV_Init(INST_LPIT1, &lpit1_InitConfig);

LPIT_DRV_InitChannel(INST_LPIT1, LPIT_CHANNEL1, &lpit1_ChnConfig0);

INT_SYS_InstallHandler(LPIT0_Ch1_IRQn, ISR_LPIT0_Ch1_1ms, (isr_t*)0);

pFunLpitCallback = NULL;
}

The APP LPIT Init code:

void LPIT_Init(void)
{
LPIT_DRV_Init(INST_LPIT1, &lpit1_InitConfig);

LPIT_DRV_InitChannel(INST_LPIT1, LPIT_CHANNEL0, &lpit1_ChnConfig0);
LPIT_DRV_InitChannel(INST_LPIT1, LPIT_CHANNEL1, &lpit1_ChnConfig1);
LPIT_DRV_InitChannel(INST_LPIT1, LPIT_CHANNEL2, &lpit1_ChnConfig2);

INT_SYS_InstallHandler(LPIT0_Ch0_IRQn, ISR_LPIT0_Ch0_1ms, (isr_t*)0);
INT_SYS_InstallHandler(LPIT0_Ch1_IRQn, ISR_LPIT0_Ch1_1ms, (isr_t*)0);
INT_SYS_InstallHandler(LPIT0_Ch2_IRQn, ISR_LPIT0_Ch2_10ms, (isr_t*)0);


LPIT_DRV_StartTimerChannels(INST_LPIT1, 1 << LPIT_CHANNEL0); //channel 0
LPIT_DRV_StartTimerChannels(INST_LPIT1, 1 << LPIT_CHANNEL1); //channel 1
LPIT_DRV_StartTimerChannels(INST_LPIT1, 1 << LPIT_CHANNEL2); //channel 2


pFunLpitCallback = NULL;
}

0 项奖励
回复
2 回复数

914 次查看
Alexis_A
NXP TechSupport
NXP TechSupport

Dear  赵 子成.

Usually when you exit a bootloader al the timers and peripherals should be deinitialize before enter your application. So I will suggest to call to stop and deinitialize the peripheral before entering your application.

Let me know if this helps you.

Best Regards,

Alexis Andalon

914 次查看
赵子成
Contributor IV

Hi , Yes, it works.

Now I call MCAL_DeInit before jump to APP:

BOOL MCAL_DeInit(void)
{
status_t status = STATUS_SUCCESS;

LPSPI_Type *base = g_lpspiBase[LPSPI_ID2];

LPIT_DRV_Deinit(INST_LPIT1);

status = status || LPSPI_Disable(base);

status = status || FLEXCAN_DRV_Deinit(INST_CANCOM1);

status = status || WDOG_DRV_Deinit(INST_WATCHDOG1);

if(status == STATUS_SUCCESS)
{
return TRUE;
}
else
{
return FALSE;
}
}

Now I deinit LPIT, SPI, CAN, WDOG module.

0 项奖励
回复