Is the LPSPI in NXP S32K144 standalone?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is the LPSPI in NXP S32K144 standalone?

ソリューションへジャンプ
566件の閲覧回数
gannyofficial
Contributor I

Hello everyone,

As per the reference manual the NXP S32K144HAMLL has 3 Low Power Serial Peripheral Interfaces operating with the clock source of SIRC. 

I would like to know whether the 3 LPSPI operate as a standalone with the clock source or not. I couldnt find the complete bus diagram showing how the clock source is connected to all the three SPI. If anyone could clarify this, will be really helpful. Thanks. 

0 件の賞賛
返信
1 解決策
548件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @gannyofficial 

The 3 LPSIs can operate with the same or different clock source (SOSC, SIRC, FIRC and SPLL) and each of these will work independently whether they share a clock source or not.
I am attaching some diagrams of the clock architecture and various clock sources for this device.

NOTE: Images obtained from S32DS ConfigTools.

VaneB_0-1666905142451.pngVaneB_1-1666905156022.png

 

B.R.

VaneB

 

元の投稿で解決策を見る

1 返信
549件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @gannyofficial 

The 3 LPSIs can operate with the same or different clock source (SOSC, SIRC, FIRC and SPLL) and each of these will work independently whether they share a clock source or not.
I am attaching some diagrams of the clock architecture and various clock sources for this device.

NOTE: Images obtained from S32DS ConfigTools.

VaneB_0-1666905142451.pngVaneB_1-1666905156022.png

 

B.R.

VaneB