EB Tresos warning for ADC module of S32K1XX

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

EB Tresos warning for ADC module of S32K1XX

1,284 次查看
shudhamatinarha
Contributor II

Hello, 

getting following warning when I reopen my ADC configuration in EB Tresos.

Configurations has no error or warnings related to ADC this warning is only popping up while opening the project and its not affecting validation or generation but want to know what warning means exactly,.

"Node /TS_T40D2M10I1R0/Adc/AdcConfigSet/AdcHwUnit/AdcGroup/AdcEnableHalfInterrupt defines two attributes with the same name "EDITABLE" which could not be merged. Removing one of the attributes"

Note: I haven't configured anything related to half interrupt.

Thank you in advance. 

0 项奖励
回复
1 回复

1,271 次查看
hungnguyenphi
NXP Employee
NXP Employee

Dear Shudhamatinarha,

This is an error in the MCAL package. This issue has been fixed in the S32K14X_MCAL4_2_RTM_1_0_4 package.

Best regards,

Hung.