Debugging issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Debugging issue

跳至解决方案
548 次查看
Ayaz
Contributor III

Hi 

I am facing an issue with S32D, when I am trying to debug,it gives me this error:

Skærmbillede 2024-04-23 105234.png

I have reinstalled the S32D and Pemiro drivers,but still have the same issue.

0 项奖励
回复
1 解答
489 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @Ayaz 

Please create a blank "S32DS Application Project" and see if you get the same error. Also, try with an example code.

Additionally, can you please try the following?

  1. Turn the switch off
  2. disconnect the 12-volts
  3. reconnect the 12-volts
  4. turn the switch on

This power-up procedure manages that SBC starts with the disabled watchdog. Four orange LEDs indicate active 12, 5, 3.3, and 1.5 V power supply domains.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
512 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @Ayaz 

What project are you flashing to the target? Is it one of the example projects or a custom one? Is this the first time you ever tried or did it work previously and now fail? Are you using custom boards? Or is it an NXP board?

 

B.R.

VaneB

0 项奖励
回复
497 次查看
Ayaz
Contributor III

Hi

This is not the first time, and I figured that the issue was from the evaluation board (S32k344 Q172), when I am switching to (S32k344 T172). I did not have this issue anymore, do you have any idea, how to fix this?

0 项奖励
回复
490 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @Ayaz 

Please create a blank "S32DS Application Project" and see if you get the same error. Also, try with an example code.

Additionally, can you please try the following?

  1. Turn the switch off
  2. disconnect the 12-volts
  3. reconnect the 12-volts
  4. turn the switch on

This power-up procedure manages that SBC starts with the disabled watchdog. Four orange LEDs indicate active 12, 5, 3.3, and 1.5 V power supply domains.

0 项奖励
回复