Connections of the EvalBoard

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Connections of the EvalBoard

772 Views
michaelw
Contributor I

Is it possible to connect the S32k144-Q100 EvalBoard to an external PowerSource (12V) via the powerJack (Switch Jumper 107) and connect the USB to the Laptop for using the Debugger?
Asking if any Leakage-Current will occure by Ground loops destroying the SBC or other parts.

Greetings and thank you in advance

Labels (1)
0 Kudos
Reply
1 Reply

649 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

Sorry for the late response,

You should be able to use USB along with SBC which requires 12V, J107(1-2). It should be protected.

Regards,

Daniel

0 Kudos
Reply