Example S32K312 CAN Transmit & Receive Using MB & FIFO DMA DS3.5 RTD300

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Example S32K312 CAN Transmit & Receive Using MB & FIFO DMA DS3.5 RTD300

Example S32K312 CAN Transmit & Receive Using MB & FIFO DMA DS3.5 RTD300

*******************************************************************************

 The purpose of this demo application is to present a usage of the
 FlexCAN IP Driver for the S32K3xx MCU.

 The example uses FLEXCAN-0 for transmit & receive Tusing following Message buffer :--
#define RX_MB_IDX_0 10U
#define RX_MB_IDX 11U
#define TX_MB_IDX 12U

FIFO Receive Message from range :--
0x01 to 0x16

BAUDRATE : 500 KBPS

 ------------------------------------------------------------------------------
* Test HW: S32K3X2EVB-Q172
* MCU: S32K312
* Compiler: S32DS3.5
* SDK release: RTD 3.0.0
* Debugger: PE micro
* Target: internal_FLASH
********************************************************************************

 

Dinesh_Guleria_0-1705388137796.png

 

附件
评论

Thanks, Very useful code

100% 有帮助 (1/1)
版本历史
最后更新:
‎01-15-2024 11:57 PM
更新人: