Hello,
I have an external micro-controller and I want the micro-controller to sent the SJA1110 Configuration over SPI to start the switch.
So can you provide the needed switch configuration to work in unmanaged mode and the needed SPI register configurations for the the switch to receive this configurations and start the switch with it.
Or if you can provide a demo for sending the configuration from a micro-controller over SPI and receiving it by the switch to start it.
Thank you
Hello,
Thank you for replaying fast.
In fact i'm not using MCX, I'm using a different board, MLSoC™ DevKit 2.0 for SIMA.AI.
And I wanted to send the switch configuration to the switch from the board over SPI during boot.
Thank you,
Hello @haidysorial
I'm not sure how to use SJA1110 with MLSoC™ DevKit 2.0.
While there is a solution about using it with our S32G product:
https://www.nxp.com.cn/docs/en/fact-sheet/SJA1110AUTESFS.pdf
If you still have question about SJA1110, recommend you submit a private ticket from:
https://www.nxp.com/support/support:SUPPORTHOME
BR
Alice
Hi @haidysorial
SJA1110 is Multi-Gig TSN Ethernet Switch, are you sure you use it with MCX? If not, which MCU do you work with it? Please let us know thus we can assign the thread to the right engineer to help you.
Thanks,
Jun Zhang