send SJA1110 switch configurations over spi

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

send SJA1110 switch configurations over spi

519 Views
haidysorial
Contributor I

Hello,

I have an external micro-controller and I want the micro-controller to sent the SJA1110 Configuration over SPI to start the switch.

So can you provide the  needed switch configuration to work in unmanaged mode and the needed SPI register configurations for the the switch to receive this configurations and start the switch with it.


Or if you can provide a demo for sending the configuration from a micro-controller over SPI and receiving it by the switch to start it. 

Thank you

0 Kudos
4 Replies

451 Views
haidysorial
Contributor I

Hello,

Thank you for replaying fast.

In fact i'm not using MCX, I'm using a different board, MLSoC™ DevKit 2.0 for SIMA.AI.
And I wanted to send the switch configuration to the switch from the board over SPI during boot.

Thank you,

0 Kudos

292 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @haidysorial 

I'm not sure how to use SJA1110 with MLSoC™ DevKit 2.0.

While there is a solution about using it with our S32G product:

https://www.nxp.com.cn/docs/en/fact-sheet/SJA1110AUTESFS.pdf 

If you still have question about SJA1110,  recommend you submit  a private ticket from:

https://www.nxp.com/support/support:SUPPORTHOME 

Alice_Yang_0-1711104974201.png

 

BR

Alice

0 Kudos

492 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi @haidysorial 

SJA1110 is Multi-Gig  TSN Ethernet Switch, are you sure you use it with MCX? If not, which MCU do you work with it? Please let us know thus we can assign the thread to the right engineer to help you.

Thanks,

Jun Zhang

0 Kudos

336 Views
haidysorial
Contributor I

Hello,

Any updates?

Haidy

0 Kudos