Where is BSP 30.0 and BSP 32.0 located? I only see BSP 28.0 posted on nxp.com

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Where is BSP 30.0 and BSP 32.0 located? I only see BSP 28.0 posted on nxp.com

2,336 次查看
PhilipPesses
NXP Employee
NXP Employee

Need links to download BSP 30 & BSP 32

标记 (1)
0 项奖励
回复
6 回复数

2,220 次查看
asap
NXP Employee
NXP Employee

John,

last week, we released GoldVIP 1.2.0 which is built based on Yocto project with BSP32. if you are interested, that is the place to start with your evaluation.

official S32G software package (consists all S32G standard software and reference software) update scheduled in coming weeks. 

Albert
0 项奖励
回复

2,312 次查看
asap
NXP Employee
NXP Employee

Phil,

please access S32G2 BSP30 through: Automotive Software Package Manager | NXP Semiconductors

BSP32 is still not yet officially released, will be out within the new bundle release by early Q3. 

Albert
0 项奖励
回复

2,303 次查看
jbirchy
Contributor IV

This repository shows BSP31 & BSP32, is that not an official release repository?

https://source.codeaurora.org/external/autobsps32/auto_yocto_bsp

Need documentation for BSP 31 & 32.

Thanks

  John

0 项奖励
回复

2,216 次查看
jbirchy
Contributor IV
0 项奖励
回复

2,202 次查看
asap
NXP Employee
NXP Employee

John,

Both BSP30 and BSP32 can be found through Code Aurora (now) and Flexera (alpha enablement account), and BSP32 will also go public through Automotive Software Package manager and Flexera (general user account) when the S32G software bundle 4 releases.

you could use the below links to access BSP32:

https://source.codeaurora.org/external/autobsps32/auto_yocto_bsp/?h=bsp32.0

hope it helps.

Albert
0 项奖励
回复

2,227 次查看
jbirchy
Contributor IV

@asapdid you see my response above?

0 项奖励
回复