Where is BSP 30.0 and BSP 32.0 located? I only see BSP 28.0 posted on nxp.com

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where is BSP 30.0 and BSP 32.0 located? I only see BSP 28.0 posted on nxp.com

2,077件の閲覧回数
PhilipPesses
NXP Employee
NXP Employee

Need links to download BSP 30 & BSP 32

タグ(1)
0 件の賞賛
返信
6 返答(返信)

1,961件の閲覧回数
asap
NXP Employee
NXP Employee

John,

last week, we released GoldVIP 1.2.0 which is built based on Yocto project with BSP32. if you are interested, that is the place to start with your evaluation.

official S32G software package (consists all S32G standard software and reference software) update scheduled in coming weeks. 

Albert
0 件の賞賛
返信

2,053件の閲覧回数
asap
NXP Employee
NXP Employee

Phil,

please access S32G2 BSP30 through: Automotive Software Package Manager | NXP Semiconductors

BSP32 is still not yet officially released, will be out within the new bundle release by early Q3. 

Albert
0 件の賞賛
返信

2,044件の閲覧回数
jbirchy
Contributor IV

This repository shows BSP31 & BSP32, is that not an official release repository?

https://source.codeaurora.org/external/autobsps32/auto_yocto_bsp

Need documentation for BSP 31 & 32.

Thanks

  John

0 件の賞賛
返信

1,957件の閲覧回数
jbirchy
Contributor IV
0 件の賞賛
返信

1,943件の閲覧回数
asap
NXP Employee
NXP Employee

John,

Both BSP30 and BSP32 can be found through Code Aurora (now) and Flexera (alpha enablement account), and BSP32 will also go public through Automotive Software Package manager and Flexera (general user account) when the S32G software bundle 4 releases.

you could use the below links to access BSP32:

https://source.codeaurora.org/external/autobsps32/auto_yocto_bsp/?h=bsp32.0

hope it helps.

Albert
0 件の賞賛
返信

1,968件の閲覧回数
jbirchy
Contributor IV

@asapdid you see my response above?

0 件の賞賛
返信