S32G274 M7 bootloader load u-boot to the specified sram address from flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32G274 M7 bootloader load u-boot to the specified sram address from flash

1,291件の閲覧回数
dengdaokuan
Contributor I

Hi

  In the project, we use the S32G274 chip, let the M core load the u-boot to the SRAM and trigger the A53 to execute.

  We divided the sram area and specified the load address of u-boot as (0x34600000 - 0x346FFFFF, 1M for u-boot), the default start address is (0x34000000).

  Based on the bsp29 version, I verified that u-boot is loaded to (0x34000000) and (0x34200000 for test) are executed without problems, but (0x34600000) does not work!!!
  Please help to confirm whether additional modifications are required in u-boot to support (0x34600000) operation, or(0x34600000) this address cannot be used for u-boot loading.
0 件の賞賛
返信
1 返信

1,237件の閲覧回数
asap
NXP Employee
NXP Employee

Dengdaokuan,

Thank you for your inquiry. Offline discussion in the past days followed by local team on going, please synchronize the info with your NXP contact to get the latest update!

Albert
0 件の賞賛
返信