S32G274 M7 bootloader load u-boot to the specified sram address from flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G274 M7 bootloader load u-boot to the specified sram address from flash

1,290 Views
dengdaokuan
Contributor I

Hi

  In the project, we use the S32G274 chip, let the M core load the u-boot to the SRAM and trigger the A53 to execute.

  We divided the sram area and specified the load address of u-boot as (0x34600000 - 0x346FFFFF, 1M for u-boot), the default start address is (0x34000000).

  Based on the bsp29 version, I verified that u-boot is loaded to (0x34000000) and (0x34200000 for test) are executed without problems, but (0x34600000) does not work!!!
  Please help to confirm whether additional modifications are required in u-boot to support (0x34600000) operation, or(0x34600000) this address cannot be used for u-boot loading.
0 Kudos
Reply
1 Reply

1,236 Views
asap
NXP Employee
NXP Employee

Dengdaokuan,

Thank you for your inquiry. Offline discussion in the past days followed by local team on going, please synchronize the info with your NXP contact to get the latest update!

Albert
0 Kudos
Reply