S32G2 with RTD 3.0.x drivers and QSPI Flash: how to disable AHB buffer ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32G2 with RTD 3.0.x drivers and QSPI Flash: how to disable AHB buffer ?

跳至解决方案
2,330 次查看
SSyb
Contributor III

Hi all,

am working on an S32G274A board (bt not one of the NXP products, it is manufactured by a 3rd party), it has a Micron
MT35XU512ABA octal serial NOR flash mounted. for the M7_0, I have to adapt the RTD/MCAL fls configuration LUT sequences, until now with mediocre success.
(current RTD version: SW32G_RTD_4.4_3.0.2_HF01)
Reading and writing the special configuration registers in STRD mode (when booting) seems to work. Then I switch to octal DDR mode, but either my write or my read sequences
fail to work correctly. No errors reported, but I can not confirm by reading back what I have just written to the flash memory.
it is not an issue wth the write enable, the RDT drivers set this automatically.

to rule out that it has something to do with the AHB buffer, I would like to disable the AHB feature (the S32G2 reference manual sugessts that there is the option between
- IP command read (I would like to try that)
- AHB read (used in all examples from NXP)

I was wondering how to disable or remove the AHB feature from my configuration (in Tresos). But removing the subcontaines in the AHB configuration yields a tool error.
--> How do I get to use a bare IP command read ?

And follow up question: are there examples with Micron flash configurations available (for the M7) ?


thanks and best regards,
Stefan

0 项奖励
回复
1 解答
2,242 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

The User Manual for the FLS driver provides information on regards of the AHB usage under a read command. The following snip is provided from the User Manual:

DanielAguirre_0-1684250137130.png

AHB can only be used under a read command, for which any write commands should not be valid through AHB. Also, the following limitation is shown under the User Manual:

"Users must add and use MPU to configure the QSPI AHB address space as device memory to prevent speculative reads in this region"

Please, let us know.

在原帖中查看解决方案

0 项奖励
回复
6 回复数
2,308 次查看
kef2
Senior Contributor V

Just use IP commands, AHB doesn't have to be disabled. 

DDR at high speeds needs special care. Data learning pattern or other means to fine tune sample point. 

0 项奖励
回复
2,277 次查看
SSyb
Contributor III

Hi @kef2 ,

understood, but if your suggestions is to use IP commands directly (in a programmatic way): I don't have that freedom. I am working on a classic AUTOSAR system with the NXP RTD driver stack acting as the AUTOSAR MCAL layer. My entry point to the flash driver is Fls_Write(), Fls_Read(), Fls_Erase() etc. Whatever is hapenning inside the driver can only be controlled through the configuration of the NXP RTD stack through the Tresos tool.

So I was wondering what to configure in Tresos / the RDT offline configuration to make it use only IP commands and ignore the AHB buffer.

best regards,

Stefan

 

标记 (1)
0 项奖励
回复
2,274 次查看
kef2
Senior Contributor V

I can't help you with Autosar, but I believe that in your situation suspect #1 is DDR mode, not AHB. Did you try reducing QSPI clock to 20MHz or even less? 

0 项奖励
回复
2,251 次查看
SSyb
Contributor III

Hi @kef2 ,

 

in the meantime I can confirm that register read, data read and page program are working in octal DDR mode, so I guess my DDR settings should be more or less correct.

And I can see these results in the AHB buffer, hence I decided to trust the AHB for the moment.

However, I don't get a sector erase to work, I have opened a different thread for this, since it is a different topic.

it @every body else out there:  it would still be interesting to know how the selection between AHB and IP access is controlled in the NXP RDT drivers withg the help of Tresos. Any hints welcome.

 

0 项奖励
回复
2,243 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

The User Manual for the FLS driver provides information on regards of the AHB usage under a read command. The following snip is provided from the User Manual:

DanielAguirre_0-1684250137130.png

AHB can only be used under a read command, for which any write commands should not be valid through AHB. Also, the following limitation is shown under the User Manual:

"Users must add and use MPU to configure the QSPI AHB address space as device memory to prevent speculative reads in this region"

Please, let us know.

0 项奖励
回复
2,227 次查看
SSyb
Contributor III

Hi @Daniel-Aguirre ,

Thank you for the hint, the checkbox in the FlsMem container I had missed (I was focused on the Fls ConrollerCfg->FlsAhbBuffer container).

To switch the AHB buffering off completely, I noticed that also the "Fls Ahb Buffer ALl Masters enable" checkbox must be disabled in the ControllerCfg contrainer (plus the one that you mentioned), then it works.

 

SSyb_0-1684308272700.png

Thx again,

best regards,

Stefan

0 项奖励
回复