QNX Hypervisor Error on s32g

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

QNX Hypervisor Error on s32g

跳至解决方案
362 次查看
lewis123
Contributor II

I am running QNX hypervisor on S32G-VNP-RDB2.

The hypervisor host can boot normally(I also built Arm Trusted firmware and uboot). But the guest failed.

Then I run "qvm-check", I get the following error:

Virtualization is available, but not enabled by the IPL.
Process 77845 (qvm-check) exited status=2.

What should I do to make the guest run properly?

0 项奖励
回复
1 解答
327 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @lewis123 

QNX hyperviser is the 3rd party software that is not developed by NXP, thus is not directly supported, we can recommend contacting the QNX support team, for them to provide you with better information that the one we can provide at this moment.
We do apologize for the inconvenience.
 
BR
Chenyin

在原帖中查看解决方案

0 项奖励
回复
2 回复数
328 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @lewis123 

QNX hyperviser is the 3rd party software that is not developed by NXP, thus is not directly supported, we can recommend contacting the QNX support team, for them to provide you with better information that the one we can provide at this moment.
We do apologize for the inconvenience.
 
BR
Chenyin
0 项奖励
回复
252 次查看
lewis123
Contributor II

Thank you.

0 项奖励
回复