QNX Hypervisor Error on s32g

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QNX Hypervisor Error on s32g

Jump to solution
358 Views
lewis123
Contributor II

I am running QNX hypervisor on S32G-VNP-RDB2.

The hypervisor host can boot normally(I also built Arm Trusted firmware and uboot). But the guest failed.

Then I run "qvm-check", I get the following error:

Virtualization is available, but not enabled by the IPL.
Process 77845 (qvm-check) exited status=2.

What should I do to make the guest run properly?

0 Kudos
Reply
1 Solution
323 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @lewis123 

QNX hyperviser is the 3rd party software that is not developed by NXP, thus is not directly supported, we can recommend contacting the QNX support team, for them to provide you with better information that the one we can provide at this moment.
We do apologize for the inconvenience.
 
BR
Chenyin

View solution in original post

0 Kudos
Reply
2 Replies
324 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @lewis123 

QNX hyperviser is the 3rd party software that is not developed by NXP, thus is not directly supported, we can recommend contacting the QNX support team, for them to provide you with better information that the one we can provide at this moment.
We do apologize for the inconvenience.
 
BR
Chenyin
0 Kudos
Reply
248 Views
lewis123
Contributor II

Thank you.

0 Kudos
Reply