QNX Hypervisor Error on s32g

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QNX Hypervisor Error on s32g

ソリューションへジャンプ
359件の閲覧回数
lewis123
Contributor II

I am running QNX hypervisor on S32G-VNP-RDB2.

The hypervisor host can boot normally(I also built Arm Trusted firmware and uboot). But the guest failed.

Then I run "qvm-check", I get the following error:

Virtualization is available, but not enabled by the IPL.
Process 77845 (qvm-check) exited status=2.

What should I do to make the guest run properly?

0 件の賞賛
返信
1 解決策
324件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @lewis123 

QNX hyperviser is the 3rd party software that is not developed by NXP, thus is not directly supported, we can recommend contacting the QNX support team, for them to provide you with better information that the one we can provide at this moment.
We do apologize for the inconvenience.
 
BR
Chenyin

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
325件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @lewis123 

QNX hyperviser is the 3rd party software that is not developed by NXP, thus is not directly supported, we can recommend contacting the QNX support team, for them to provide you with better information that the one we can provide at this moment.
We do apologize for the inconvenience.
 
BR
Chenyin
0 件の賞賛
返信
249件の閲覧回数
lewis123
Contributor II

Thank you.

0 件の賞賛
返信