Is S32G SAF software component able to run on the A53 core?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is S32G SAF software component able to run on the A53 core?

351件の閲覧回数
marvin_wang
Contributor I

Hi NXP experts 

 

In our system architecture we wish to only use S32G A53 core for safety critical applications and wish to keep M7 cores down. So i am woundering if the SAF software are designed to be run on A53 cores as well? 

we saw in the intruduction page of SAF, it shows it supports both M7 and A53 but in the evaluation package we only found example projects for M7, is the code identical for both processors? 

marvin_wang_0-1709962489393.png

 

thanks 

Marvin 

0 件の賞賛
返信
1 返信

296件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Thanks for the questions

Well, the SAF is a premium software. since this is a public channel, we recommend going directly to your local NXP representative/FAE.

 

Regarding to the SAF, the current released code is targeted running on M7 cores, which is described below:

chenyin_h_1-1710232053259.png

 

You may reference the following document for the details.

https://www.nxp.com/webapp/Download?colCode=TP-INTRO-S32G-SOFT-OFFE

 

As mentioned, we do recommend taking these inquiries to your local NXP representative/FAE for them to channel it through the correct medium.

Sorry for your inconvenience.

 

Best Regards

Chenyin

0 件の賞賛
返信