Does the S32R45 support PCIe NVMe SSDs?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does the S32R45 support PCIe NVMe SSDs?

ソリューションへジャンプ
971件の閲覧回数
amei_liu
Contributor II

hardware: S32R45 EVB

                Crucial P3 1TB PCIe M.2 2280 SSD

I connect this SSD to the PCI interface of the EVB through an M.2 to PCIE cable.As follow:

11.png

 

After the EVB board is started, enter the following command in the shell interface:

222.png

 

タグ(1)
0 件の賞賛
返信
1 解決策
899件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hello, 

Yes, it does. The connector you are using is configured by default to work as EP, not RC. 

There are a few things to take into account like the clock and the EP/RC configuration in the BSP.

There are more details on how to get that port working as RC here

https://community.nxp.com/t5/Other-NXP-Products/S32R45-Does-PCIe1-work-as-Root-Complex-mode-on-the-S...

Saludos,

Alejandro

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
900件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hello, 

Yes, it does. The connector you are using is configured by default to work as EP, not RC. 

There are a few things to take into account like the clock and the EP/RC configuration in the BSP.

There are more details on how to get that port working as RC here

https://community.nxp.com/t5/Other-NXP-Products/S32R45-Does-PCIe1-work-as-Root-Complex-mode-on-the-S...

Saludos,

Alejandro

 

0 件の賞賛
返信