Couldnt insert one of the kernel modules in IPCF address already in use error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Couldnt insert one of the kernel modules in IPCF address already in use error

553 Views
ashwini2024
Contributor II

S32G3

BSP 40.0

IPCF 4.10

On m core side: AUTOSAR

On a core :Linux

0 Kudos
Reply
3 Replies

538 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Can you help us elaborate more on regards of the setup you are doing? Which commands are you inputting under uboot? Can you help us sharing the whole boot log of your system?

Is the BSP being built manually with yocto? Or are you using the pre-built images provided by NXP?

Please, let us know.

0 Kudos
Reply

471 Views
ashwini2024
Contributor II

The below is the boot loG. WE are manually building and not pre built images.

0 Kudos
Reply

460 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for your feedback. We can recommend using the pre-built images by NXP to isolate any compilation/configuration errors under your custom build. The following community post provides information on regards of manually building the IPCF module and loading into a pre-built image by NXP:

Re: Issue with NXP S32G274A RDB2 -  IPCF - NXP Community

Please, let us know.

0 Kudos
Reply