Build failed on BSP40 with enabling secboot feature.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Build failed on BSP40 with enabling secboot feature.

ソリューションへジャンプ
628件の閲覧回数
Jeff-CF-Huang
Contributor II

Hi Sir

I enable secboot feature like this.

DISTRO_FEATURES:append = " pfe hse secboot"

I encountered a build error.

Could you help me check it?

JeffCFHuang_0-1714989533384.png

 

0 件の賞賛
返信
1 解決策
581件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, thanks for the reply.

If you do not want to remove corresponding 3 files mentioned from previous post, the following method may also be useful, add the following line to conf/local.conf, then rebuild:

PREFERRED_VERSION_arm-trusted-firmware-tools-native = "2.5"

 

Hope it helps.

 

Best Regards

Chenyin

元の投稿で解決策を見る

3 返答(返信)
582件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, thanks for the reply.

If you do not want to remove corresponding 3 files mentioned from previous post, the following method may also be useful, add the following line to conf/local.conf, then rebuild:

PREFERRED_VERSION_arm-trusted-firmware-tools-native = "2.5"

 

Hope it helps.

 

Best Regards

Chenyin

607件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, Thanks for the question

  1. To enable SECBoot Support, update the conf/local.conf file in the Yocto build directory with these lines:

DISTRO_FEATURES:append = " secboot"

NXP_FIRMWARE_LOCAL_DIR = "/path/to/firmware/folder"

Enabling HSE Secure Boot in the conf/local.conf file will automatically enable PKCS11 Support & HSE Linux Driver as well. You may not need to add additional “hse” here.

  1. For the building error, since only TF-A 2.5 is used in BSP40, you may temporally remove the TF-A 2.10 related files under sources/meta-alb/recipes-bsp/arm-trusted-firmware/ as a workaround.

Hope it helps.

 

Best Regards

Chenyin

0 件の賞賛
返信
605件の閲覧回数
Jeff-CF-Huang
Contributor II

Hi Sir,
Can TF-A 2.10 be disregarded without being deleted?

0 件の賞賛
返信