Hello,
I reiceived the S32G-VNP-GLDBOX, boot by SD, power on and get the boot log through UART, but when I can't see pfe0/1/2 through ifconfig, and whitch phy is eth0? what should I do if I want to ping through ETH interface?
root@s32g274ardb2:/etc# ifconfig
eth0: flags=4099<UP,BROADCAST,MULTICAST> mtu 1500
inet6 fe80::c04c:a4ff:fee9:244b prefixlen 64 scopeid 0x20<link>
ether c2:4c:a4:e9:24:4b txqueuelen 1000 (Ethernet)
RX packets 18 bytes 1080 (1.0 KiB)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 18 bytes 2757 (2.6 KiB)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
device interrupt 63 base 0x2000
lo: flags=73<UP,LOOPBACK,RUNNING> mtu 65536
inet 127.0.0.1 netmask 255.0.0.0
inet6 ::1 prefixlen 128 scopeid 0x10<host>
loop txqueuelen 1000 (Local Loopback)
RX packets 82 bytes 6220 (6.0 KiB)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 82 bytes 6220 (6.0 KiB)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
U-Boot 2020.04+gf30287c440 (Nov 29 2022 - 16:57:39 +0000)
CPU: NXP S32G274A rev. 2.1
Model: NXP S32G274A-RDB2
DRAM: 3.5 GiB
Ignore unsupported SCMI protocol 19
MMC: FSL_SDHC: 0
Loading Environment from MMC... OK
Configuring PCIe0 as RootComplex
PCIe0: Failed to get link up
PCI: Failed autoconfig bar 20
PCI: Failed autoconfig bar 24
In: serial@401c8000
Out: serial@401c8000
Err: serial@401c8000
Board revision: RDB3 Revision E
Net: EQOS phy: rgmii @ 1
Welcome to Auto Linux BSP 35.0 (gatesgarth)!
Solved! Go to Solution.
Thanks for the reply
I suggest reading the chapter7 of BSP35UM in advance, it detailed described the settings/usage of the GMAC/PFE under u-boot/Linux.
Hope it helps.
Best Regards
Chenyin
Thanks for the reply
I suggest reading the chapter7 of BSP35UM in advance, it detailed described the settings/usage of the GMAC/PFE under u-boot/Linux.
Hope it helps.
Best Regards
Chenyin
Hello, @yangjinzhuang
Thanks for the question.
In general, eth0 is the GMAC port, would you please share the following two results?
There should be pfex which stand for the PFE related ports
Best Regards
Chenyin
Hello,
If I build linux-BSP source code myself, there are some targets choise as follow.
1、what is target fsl-image-networking or fsl-image-networking-full ?
2、what is the difference between fsl-image-networking and fsl-image-networking-full?
3、which target is for PFE include?
4、where can I get the PFE user manual doc?
You can now run 'bitbake <target>'
Targets specific to NXP:
fsl-image-mfgtool-initramfs
fsl-image-itb
fsl-image-blueboxdt
fsl-image-auto
fsl-image-bluebox
fsl-image-networking
fsl-image-dom0less
fsl-image-flash
fsl-image-blueboxsdfactory
fsl-image-base
fsl-image-blueboxbootflash
fsl-image-ubuntu-base
fsl-image-ubuntu-ros
fsl-image-fit
fsl-image-base-fit
fsl-image-itbflash
fsl-image-networking-full
fsl-image-ubuntu
fsl-image-sim
To return to this build environment later please run:
.