SJA1110 SDK in S32DS 3.4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SJA1110 SDK in S32DS 3.4

873 Views
mhjo
Contributor I

Hi. I'm using S32DS 3.4 for SJA1110 SDK.

I Add SDK .zip file in 'Abailable S32DS Software Sites' for 'Preferences -> S32 Design Studio for S32 Platform -> S32DS Extensions and Updates'

but I couldn't find any related packages in 'Help -> S32DS Extensions and Updates'

What should I do?

SDK name : com.nxp.s32ds.sja1110.composite_1.0.0.20210319172717.zip
S32DS version : 3.4
OS version : Ubuntu 18.04.6 LTS

Labels (1)
2 Replies

847 Views
RachelGomez123
Contributor I

If you have added the SDK .zip file to the "Available S32DS Software Sites" in your preferences, you should be able to see the related packages in the "S32DS Extensions and Updates" window. If you are unable to find the related packages, there may be a few things you can try:

Make sure you have selected the correct update site in the "S32DS Extensions and Updates" window. Sometimes, if you have multiple update sites, the packages you are looking for may be available in a different site.

Check if the SDK .zip file you have downloaded is compatible with S32DS version 3.4. You may need to download a different version of the SDK if it is not compatible with your S32DS version.

Check if there are any network or firewall issues that may be preventing S32DS from connecting to the update site. You can try temporarily disabling your firewall or antivirus software to see if it resolves the issue.

If you have tried these steps and are still unable to find the related packages, you may want to contact NXP support for further assistance.

 

Regards,

Rachel Gomez

0 Kudos
Reply

867 Views
viswa_kondapall
Contributor IV

Me also facing same problem. com.nxp.s32ds.sja1110.composite_1.0.0.20210319172717.zip dosent in S32DS 3.4 . 

Release note is clearly says what RTD version need to use etc details clearly mentioned.

it is compatible with S32DS3.5. In S32ds 3.5 it is not loading but saying some error.

0 Kudos
Reply