S32K3 EB tresos29 no Lauterbach debugger

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3 EB tresos29 no Lauterbach debugger

Jump to solution
585 Views
harryoceana
Contributor II

id9527_1-1699336563470.png

I don't have a Lauterbach debugger and I can't install Trace32 software. What if I only use jlink debugging?

0 Kudos
Reply
1 Solution
562 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Yes, the examples contain sample make files which use Trace32 to load a project to microcontroller and to debug it. If you don't have Trace32., it's necessary to update the make files accordingly. We do not have the files for jlink. It's up to customers to modify the make files if different setup is used.

View solution in original post

0 Kudos
Reply
3 Replies
567 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @harryoceana 

it's not mandatory to use Trace32. You can use any debugger which supports this device.

Regards,

Lukas

0 Kudos
Reply
565 Views
harryoceana
Contributor II

I was prompted to select T32 when using make build, but I don't have the software.

1715578249917.png

0 Kudos
Reply
563 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Yes, the examples contain sample make files which use Trace32 to load a project to microcontroller and to debug it. If you don't have Trace32., it's necessary to update the make files accordingly. We do not have the files for jlink. It's up to customers to modify the make files if different setup is used.

0 Kudos
Reply