S32K3 EB tresos29 no Lauterbach debugger

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K3 EB tresos29 no Lauterbach debugger

跳至解决方案
583 次查看
harryoceana
Contributor II

id9527_1-1699336563470.png

I don't have a Lauterbach debugger and I can't install Trace32 software. What if I only use jlink debugging?

0 项奖励
回复
1 解答
560 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Yes, the examples contain sample make files which use Trace32 to load a project to microcontroller and to debug it. If you don't have Trace32., it's necessary to update the make files accordingly. We do not have the files for jlink. It's up to customers to modify the make files if different setup is used.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
565 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @harryoceana 

it's not mandatory to use Trace32. You can use any debugger which supports this device.

Regards,

Lukas

0 项奖励
回复
563 次查看
harryoceana
Contributor II

I was prompted to select T32 when using make build, but I don't have the software.

1715578249917.png

0 项奖励
回复
561 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Yes, the examples contain sample make files which use Trace32 to load a project to microcontroller and to debug it. If you don't have Trace32., it's necessary to update the make files accordingly. We do not have the files for jlink. It's up to customers to modify the make files if different setup is used.

0 项奖励
回复