S32 Design Studio for S32 Platform 3.5安装问题

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design Studio for S32 Platform 3.5安装问题

1,662件の閲覧回数
ZengXing566
Contributor I

无法在线激活,提示“Error creating activation handle.(FNP error 50003,71000,10103)”

0 件の賞賛
返信
5 返答(返信)

1,313件の閲覧回数
aruiruirui
Contributor I

Hello, I encountered another issue while installing S32DSv3.5: you do not have enough windows permission.
But I am certain that I am running the installation package as an administrator.
The following is the problem log:
Install Uninstaller: S32 Design Studio for S32 Platform 3.5 (Install All Uninstaller Components)
Status: Error
Additional Notes: Error - Error writing
My activation code: 8794-2EE1-642A-E405
Thank you!

 

 

Install Uninstaller: S32 Design Studio for S32 Platform 3.5(Install All Uninstaller Components)
Status: ERROR
Additional Notes: ERROR - Error writing

 

0 件の賞賛
返信

1,661件の閲覧回数
ZengXing566
Contributor I

ZengXing566_0-1697450269613.png

 

0 件の賞賛
返信

623件の閲覧回数
qhz
Contributor I

我也是你这个问题,你现在解决了吗

0 件の賞賛
返信

1,624件の閲覧回数
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @ZengXing566 , 

 

Please can you provide the installation log from S32DS installation directory. 

 

C:\NXP\S32DS.3.5\_S32 Design Studio for S32 Platform 3.5_installation\Logs

(or wherever your S32DS installation is located. ) 

 

Also, please can you share the activation code to check for the issue. 

 

By the time, you can try the troubleshooting guide if that works for you. 

 

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/Troubleshooting-Activation-fails-with-...

 

Thank you. Kind regards. 

 

-Mehul Patel

 

0 件の賞賛
返信

1,586件の閲覧回数
ZengXing566
Contributor I

您好!

我无法打开.log文件,看不到里面的内容。

Thank you. Kind regards.

-ZengXing

0 件の賞賛
返信