无法在线激活,提示“Error creating activation handle.(FNP error 50003,71000,10103)”
Hello, I encountered another issue while installing S32DSv3.5: you do not have enough windows permission.
But I am certain that I am running the installation package as an administrator.
The following is the problem log:
Install Uninstaller: S32 Design Studio for S32 Platform 3.5 (Install All Uninstaller Components)
Status: Error
Additional Notes: Error - Error writing
My activation code: 8794-2EE1-642A-E405
Thank you!
Install Uninstaller: S32 Design Studio for S32 Platform 3.5(Install All Uninstaller Components)
Status: ERROR
Additional Notes: ERROR - Error writing
Hi, @ZengXing566 ,
Please can you provide the installation log from S32DS installation directory.
C:\NXP\S32DS.3.5\_S32 Design Studio for S32 Platform 3.5_installation\Logs
(or wherever your S32DS installation is located. )
Also, please can you share the activation code to check for the issue.
By the time, you can try the troubleshooting guide if that works for you.
Thank you. Kind regards.
-Mehul Patel
您好!
我无法打开.log文件,看不到里面的内容。
Thank you. Kind regards.
-ZengXing