Port S32DS ARM project to S32DS Power PC v1.2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Port S32DS ARM project to S32DS Power PC v1.2

798件の閲覧回数
yalamandadosaky
Contributor V

Hi All , I have some sample project for S32DS V1.2 ARM and I want to import it into S32ds V1.2 Power pc , I have tried , but it is always failing at the subdir.mk files 

make: *** target pattern contains no '%'. Stop. subdir.mk
make: *** target pattern contains no '%'. Stop. subdir.mk

タグ(3)
0 件の賞賛
返信
1 返信

647件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi,

I'm afraid the migration form S32DS ARM into S32DS Power is not supported. I'd suggest you to create a new project in S32ds Power and transfer the source source files manually.

If you use S32 SDK you'd have to re-create project from scratch and add your custom code section into the new project.

Regards,

Stan 

0 件の賞賛
返信