Port S32DS ARM project to S32DS Power PC v1.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Port S32DS ARM project to S32DS Power PC v1.2

797 Views
yalamandadosaky
Contributor V

Hi All , I have some sample project for S32DS V1.2 ARM and I want to import it into S32ds V1.2 Power pc , I have tried , but it is always failing at the subdir.mk files 

make: *** target pattern contains no '%'. Stop. subdir.mk
make: *** target pattern contains no '%'. Stop. subdir.mk

0 Kudos
Reply
1 Reply

646 Views
stanish
NXP Employee
NXP Employee

Hi,

I'm afraid the migration form S32DS ARM into S32DS Power is not supported. I'd suggest you to create a new project in S32ds Power and transfer the source source files manually.

If you use S32 SDK you'd have to re-create project from scratch and add your custom code section into the new project.

Regards,

Stan 

0 Kudos
Reply