I have just upgraded to S32DS version 3.5 and have setup my pins and drivers.
I have generated the necessary files but when I try and compile I get the following error message:
Std_Types.h: No such file or directory
This file is included in one of the generated files Port_Ci_Port_Lp.h
/*==================================================================================================
* Project : RTD AUTOSAR 4.7
* Platform : CORTEXM
* Peripheral : PORT_CI
* Dependencies : none
*
* Autosar Version : 4.7.0
* Autosar Revision : ASR_REL_4_7_REV_0000
* Autosar Conf.Variant :
* SW Version : 2.0.0
* Build Version : S32K1_RTD_2_0_0_D2308_ASR_REL_4_7_REV_0000_20230804
*
* Copyright 2020-2023 NXP Semiconductors
*
* NXP Confidential. This software is owned or controlled by NXP and may only be
* used strictly in accordance with the applicable license terms. By expressly
* accepting such terms or by downloading, installing, activating and/or otherwise
* using the software, you are agreeing that you have read, and that you agree to
* comply with and are bound by, such license terms. If you do not agree to be
* bound by the applicable license terms, then you may not retain, install,
* activate or otherwise use the software.
==================================================================================================*/
#ifndef PORT_CI_PORT_IP_H
#define PORT_CI_PORT_IP_H
/**
* @file Port_Ci_Port_Ip.h
*
* @defgroup Port_IPL Port IPL
* @{
*/
#if defined(__cplusplus)
extern "C" {
#endif
/*==================================================================================================
* INCLUDE FILES
* 1) system and project includes
* 2) needed interfaces from external units
* 3) internal and external interfaces from this unit
==================================================================================================*/
#include "Std_Types.h"
#include "Port_Ci_Port_Ip_Cfg.h"
#include "Port_Ci_Port_Ip_Types.h"
#include "Port_Ci_Port_Ip_Defines.h"
#include "Devassert.h"
What am I doing wrong?
Version 3.5 feels like a massive backward step from 3.4 which was super easy to use
Andy