Installing S32 Design Studio failure

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Installing S32 Design Studio failure

1,851件の閲覧回数
daemangpark
Contributor I

Hi.

I'd been developing s32k MCU project with the S32DS.
But It happened to make error message when the s32ds exercution today.
So I deleted it and tried to re install S32DS. But it failed all tries.

Error messages are as belows

Installation: Unsuccessful.

44 Successes
6 Warnings
1 NonFatalErrors
1 FatalErrors

cll_app.dll: Can't find dependent libraries

Please check the logs I attached.
Thanks
BR

タグ(3)
0 件の賞賛
返信
1 返信

1,694件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello daemangpark‌,

Please ensure you have the Administrator privileges on your PC. As per the installation instructions, it is required to install this tool.

pastedImage_1.png

Hope it helps,

Mike

0 件の賞賛
返信