Hello, I'm using nxp mcu using s32ds 3.4. At some point, I was coding with a C file to see if I touched the settings wrong, and when I pressed the PERIPHERALS button at the top left, it not only sets the SDK function, but also follows the C file that I was coding. Also, if you set the SDK function and then press the C/C++ icon again to return to the part where you write the code, the previous SDK part will follow.
I used to use each as a separate space before, but I don't know why it's following. Is there a setting I can fix?
解決済! 解決策の投稿を見る。