Hi NXP team,
We are using S32K344 EVK board and S32 design studio v3.5.
We want to use Clock_Ip_GetClockFrequency() function from ..../RTD/include/Clock_Ip.h file to calculate time in millisecs as per below code.
void BCC_MCU_WaitMs(uint16_t delay)
{
g_sysClk = (g_sysClk) ? g_sysClk : BCC_MCU_GetSystemClockFreq();
uint32_t cycles = (uint32_t) BCC_GET_CYCLES_FOR_MS(1U, g_sysClk);
/* Advance to next multiple of 4. Value 0x04U ensures that the number
* is not zero. */
cycles = (cycles & 0xFFFFFFFCU) | 0x04U;
for (; delay > 0U; delay--) {
BCC_WAIT_FOR_MUL4_CYCLES(cycles);
}
}
But in my SDK the Clock_Ip_GetClockFrequency() function is not enabled. How to enable this function?(Please find the attached image for your reference)
Please assist me to resolve this issue.
Thanks and regards,
Hareesh
Solved! Go to Solution.
Hi @Hareesh
To enable the get clock frequency API, you have to activate it in the clock tool of Config Tools.
B.R.
VaneB
Hi @Hareesh
To enable the get clock frequency API, you have to activate it in the clock tool of Config Tools.
B.R.
VaneB