problem with pwm module of mc9s12dg25b !

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

problem with pwm module of mc9s12dg25b !

1,583 Views
jeffzxg
Contributor I
hi
   I have a problem with pwm module  of mc9s12dg256. if pwm waveform is closed by PWME register, does the output of pwm module have fixed output (high level or low level output, that decided by the output level when PWME is set to 0), or have other output state?
                                                                                                        thanks!
Labels (1)
0 Kudos
Reply
1 Reply

831 Views
kef
Specialist I
When PWM bit is clear, then corresponding data direction and port register bits (DDRP and PTP probably) determine the state of pin.
 
0 Kudos
Reply