Hello,
I hate to "Bump" a dormant topic, but I, too, would like to know about the "scratch RAM."
Is it used by the flash module internally, or might it be available to store a copy of a sector for erasure and reprogramming?
I also noticed that in Table 13-5, page 431:
Global Address | Size (Bytes) | Description
0x0_5800 – 0x0_5AFF | 768 | Memory Controller Scratch RAM (RAMON(1) = 1)
that RAMON has a footnote:
1. MMCCTL1 register bit
but the only other locations this register is mentioned are Revision Histories, page 2 and page 107:
Removed reference to MMCCTL1 register from Table 13-5
Removed references to the MMCCTL1 register
(of course the first mention is blatantly wrong)
It seems to me that this could be a unimplemented feature that evaded proofreading, but I want to know for sure.
Regards,
Michael