S12G48的时钟PLL问题

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S12G48的时钟PLL问题

跳至解决方案
1,171 次查看
huangmingsong
Contributor III
问题1:PLL的时钟偏差1.4%是否包含振荡器制造工艺、老化、温度和基频偏差,如不包含请分别提供。
问题2:能否提供超过 5us 的 PLL 抖动?
Catch0F83(04-08-(04-08-15-43-49).jpg
0 项奖励
回复
1 解答
1,132 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

A1: Yes it includes everything also including safety range for presented data. The range is not a public info but it is high enough to include all possible input factors.

A2: There is no theory related to this question. All possible data are presented in the data sheet. The data consist also safety ranges. Everything can be better but there is no guarantee for it as well as there is no procedure how to do it because it would work against presented data in the data sheet – which are guaranteed in entire range of temperatures, voltages and frequencies. Each engineer should work with worst case scenario to consider all possible conditions.

Best regards,

Ladislav

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,133 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

A1: Yes it includes everything also including safety range for presented data. The range is not a public info but it is high enough to include all possible input factors.

A2: There is no theory related to this question. All possible data are presented in the data sheet. The data consist also safety ranges. Everything can be better but there is no guarantee for it as well as there is no procedure how to do it because it would work against presented data in the data sheet – which are guaranteed in entire range of temperatures, voltages and frequencies. Each engineer should work with worst case scenario to consider all possible conditions.

Best regards,

Ladislav

0 项奖励
回复
1,139 次查看
huangmingsong
Contributor III

有人知道吗?请帮忙解答下,谢谢。

0 项奖励
回复