HCS12X Flexray Starter Kit - Connecting to Flexcard

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HCS12X Flexray Starter Kit - Connecting to Flexcard

3,472 Views
brian_s
Contributor I
Hi, 

I am currently using the flexray starter kit based on the MC9S12XDP512 and the 4300 Daughter card. I have Flexray up and running using the application example which came with the kit, and can see the data through the FREEMaster software. I am now trying to use a Flexcard (Cyclone by TZM) and CANalyzer to monitor the traffic on the network. I have already tried to edit the config file using the data in the user guide for the application example, but cannot maintain synchronisation with the flexray network. Has anyone here used CANalyzer to minitor Flexray before? Is there a config file that I could use for this?

I have used CANalyzer to connect to the CAN nodes on the starter kit, and have found that the documented information for the CAN example was incorrect. Its for this reason that I would like to get a config file for CANalyzer that is known to work with the starter kits and Flexray application example. Any help you have on this would be much appreciated

Regards
Brian
Labels (1)
0 Kudos
Reply
3 Replies

1,140 Views
Alban
Senior Contributor II
Hello,

CAN and FlexRay are different protocols with different physical interfaces, different principles...

I don't believe you can use the CANanalyzer on anything else but CAN network.

To get support on CANanalyzer, you need to contact Vector Informatik.

Cheers,
Alban.
0 Kudos
Reply

1,140 Views
brian_s
Contributor I
Sorry, I may not have been clear in my last post. I am aware that CAN and Flexray are two totally different protocols, and I have the add on to CANalyzer which supports the use of the Flexcard. The Flexcard is connecting to the Flexray network, and I am able to retrieve some of the data from the network, but it looses synchronisation very quickly. What I am looking for is the settings I need to apply to the CANalyser software to let it communicate with the network,  i.e. the configuration settings which freescale have set up the flexray application example with. I have found some of these in the freescale user manual, but there are some which I cant seem to find.

here are the paramaters that need to be filled: (i have values for some of these, but wanted to make sure they are correct, because as I said earlier the CAN application example was not as stated)

                        
 Baudrate                         
 BusGuardianTick                  
 ExternalClockCorrectionMode     
 PhysicalLayer                  
 gColdStartAttempts               
 gListenNoise                     
 gMacroPerCycle                   
 gMaxWithoutClockCorrectionFatal  
 gMaxWithoutClockCorrectionPassive
 gNetworkManagementVectorLength   
 gNumberOfMinislots             
 gNumberOfStaticSlots            
 gOffsetCorrectionStart        
 gPayloadLengthStatic            
 gSyncNodeMax                   
 gdActionPointOffset            
 gdDynamicSlotIdlePhase           
 gdMacrotick                     
 gdMinislot                     
 gdMinislotActionPointOffset    
 gdNIT                          
 gdStaticSlot                   
 gdSymbolWindow                  
 gdTSSTransmitter               
 gdWakeupSymbolRxIdle            
 gdWakeupSymbolRxLow            
 gdWakeupSymbolRxWindow          
 gdWakeupSymbolTxIdle            
 gdWakeupSymbolTxLow            
 pAllowHaltDueToClock           
 pAllowPassiveToActive          
 pChannels                        
 pClusterDriftDamping         
 pDecodingCorrection           
 pDelayCompensation[A]          
 pDelayCompensation[B]           
 pDynamicSegmentEnable         
 pExternOffsetCorrection       
 pExternRateCorrection         
 pKeySlotUsedForStartup        
 pKeySlotUsedForSync            
 pLatestTx                      
 pMacroInitialOffset[A]         
 pMacroInitialOffset[B]        
 pMaxPayloadLengthDynamic       
 pMicroInitialOffset[A]         
 pMicroInitialOffset[B]         
 pMicroPerCycle                
 pMicroPerMacroNom                
 pOffsetCorrectionOut             
 pRateCorrectionOut               
 pSamplesPerMicrotick             
 pSingleSlotEnabled               
 pWakeupChannel                   
 pWakeupPattern                   
 pdAcceptedStartupRange           
 pdListenTimeout                  
 pdMaxDrift                       
 pdMicrotick  




Has anybody used CANalyser/Flexcard for Flexray?
0 Kudos
Reply

1,140 Views
Zanzo
Contributor I

Hi, I am using the CANalyzer with the vector VN3600.

If your have two nodes that talk correctly you can put the CANalyzer in asynchronous mode. On the VN3600 this works has a monitor of the line and finds the configuration information required in order to synchronize with the nodes.

If you use the synchronous mode the vector card has to simulate a node and this is more complicated, you need to use capl and program the card in order to send synchronization frames.

Alternatively you could use the mixed mode...

0 Kudos
Reply