load .ko on ls1012afrwy

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

load .ko on ls1012afrwy

793 Views
icarus
Contributor I

When I am trying to load a pcie moule on board ls1012afrwy.

It reminds that "module format invalid"

The moudle is compiled with linux kernel 4.9.62 .

I want to ask that:

1.Which kind of .ko is matched for the board?

2.Would the board work If I change the BSP system on it to linux 4.9.62?

0 Kudos
Reply
1 Reply

706 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello YunFeng Yue,

Please generate Kernel image running on the target board and module (.ko) from the Linux Kernel source(building).

We provided LSDK to support ls1012afrwy, the latest LSDK 1812  provides Linux Kernel 4.9.140, you could run the command "flex-builder -c linux:linux:LSDK-18.12-V4.9 -a arm64" to get Linux Kernel source in the folder <install folder>/flexbuild_lsdk1812/packages/linux/linux, compilation folder in /home/yiping/flexbuild_lsdk1812/build/linux/linux/arm64/LS/output/LSDK-18.12-V4.9/.

You could compile Kernel module and Image against this version Linux Kernel.

Thanks,

Yiping

0 Kudos
Reply