To whom it may concern,
We're trying to bring up a custom board derived from the T1042 and T2081 Reference boards.
We've used the QorIQ SDK 2.0 to generate images ready to burn onto the flash.
Config pins are set for the "Hardcoded RCW" option, and we've confirmed that the Board comes out of HReset waiting for the JTAG.
How do we set up Codewarrior to use the products from the SDK to program the Flash?
Thanks for your help,
Kyle
Test your board using simple CodeWarrior program example.
Use CodeWarrior wizard for simple example creation.
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Look at the Section 5.2.2 of NXP SDK 2.0-1703 documentation:
http://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf
This Section contains list of instructions for system recovering using CodeWarrior Flash Programmer.
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Pavel,
Any thoughts? Is there any information from my end that might be helpful?
Thanks,
Kyle
Pavel,
I'm getting the following error:
CCSProtocolPlugin : Failed to correctly configure the JTAG chain
This occurs with both the flashing task and the running debug on the connection.
Thnaks,
Kyle
Pavel,
After Powercycling the Target board I'm getting a new error
CCSProtocolPlugin : Secure debug violation
CodeWarrior TAP is most recent, CW for PA is 10.5.1 eval version.
EDIT::
The following is from the Console
JTAG Diagnostics
Starting Power at Probe test ...
Test result: PASSED
Starting IR Scan test ...
Test result: PASSED
Starting Bypass Scan test ...
Test result: PASSED
Starting Arbitrary TAP State Move test ...
Test result: PASSED
Detected JTAG IDCODEs: OK
Device 0 IDCODE: 0x118E601D
ccs_jtag_unlock
serverh = 4
cc = 0
ccs_jtag_unlock; ccs_error = 0 [completed correctly]
ccs_config_chain
serverh = 4
cc = 0
device_list: (size = 1)
device[0]:: core_type=T2080(242)
ccs_config_chain; ccs_error = 39
Error message:
ccs_get_subcore_error
serverh = 4
cc = 0
error = 57
chain_pos = 0
ccs_get_subcore_error; ccs_error = 0; duration=0 ms
ccs_kill_server
serverh = 4
ccs_kill_server; ccs_error = 0
Thanks,
Kyle