T2080 IFC_CLK max frequency

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

T2080 IFC_CLK max frequency

跳至解决方案
932 次查看
gregbuchannan
Contributor I

The T2080 datasheet specifies the maximum frequency for IFC_CLK is 100 MHz.  However the T2080RDB-PC Reference Design Board U-Boot header reports IFC: 149.985 MHz.  What is the true maximum frequency of IFC_CLK?

Greg

0 项奖励
回复
1 解答
807 次查看
ufedor
NXP Employee
NXP Employee

T2080 has the maximum frequency of IFC_CLK =100MHz.

Measured IFC_CLK on T2080RDB using oscilloscope is 75MHz. The U-Boot IFC frequency indication code has to be corrected.

在原帖中查看解决方案

0 项奖励
回复
1 回复
808 次查看
ufedor
NXP Employee
NXP Employee

T2080 has the maximum frequency of IFC_CLK =100MHz.

Measured IFC_CLK on T2080RDB using oscilloscope is 75MHz. The U-Boot IFC frequency indication code has to be corrected.

0 项奖励
回复