The T2080 datasheet specifies the maximum frequency for IFC_CLK is 100 MHz. However the T2080RDB-PC Reference Design Board U-Boot header reports IFC: 149.985 MHz. What is the true maximum frequency of IFC_CLK?
Greg
解決済! 解決策の投稿を見る。
T2080 has the maximum frequency of IFC_CLK =100MHz.
Measured IFC_CLK on T2080RDB using oscilloscope is 75MHz. The U-Boot IFC frequency indication code has to be corrected.
T2080 has the maximum frequency of IFC_CLK =100MHz.
Measured IFC_CLK on T2080RDB using oscilloscope is 75MHz. The U-Boot IFC frequency indication code has to be corrected.