T2080 IFC_CLK max frequency

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T2080 IFC_CLK max frequency

Jump to solution
930 Views
gregbuchannan
Contributor I

The T2080 datasheet specifies the maximum frequency for IFC_CLK is 100 MHz.  However the T2080RDB-PC Reference Design Board U-Boot header reports IFC: 149.985 MHz.  What is the true maximum frequency of IFC_CLK?

Greg

0 Kudos
Reply
1 Solution
805 Views
ufedor
NXP Employee
NXP Employee

T2080 has the maximum frequency of IFC_CLK =100MHz.

Measured IFC_CLK on T2080RDB using oscilloscope is 75MHz. The U-Boot IFC frequency indication code has to be corrected.

View solution in original post

0 Kudos
Reply
1 Reply
806 Views
ufedor
NXP Employee
NXP Employee

T2080 has the maximum frequency of IFC_CLK =100MHz.

Measured IFC_CLK on T2080RDB using oscilloscope is 75MHz. The U-Boot IFC frequency indication code has to be corrected.

0 Kudos
Reply