Hi,
We are using LS1012a to design our custom board. So we what to understand the functional role of packet forwarding engine. We are referring "Packet Forwarding Engine.pdf" document to understand the functionality. But it we are not getting the exact functionality.
So please help us to understand PFE
Regards
Minal
Hello Minal Nemade,
LS1012A users a hardware packager forwarding engine to provide higher performance Ethernet interfaces.
The device includes two Ethernet ports. Both Ethernet ports support SGMII.
Please refer to https://freescale.sdlproducts.com/LiveContent/web/pub.xql?action=home&pub=LS1012A%20Offtrain%20SDK%2... for PFE networking driver high level decomposition and data flow.
You refer to the following application notes.
Packet Forwarding Engine (PFE) Ethernet Ports Setting up on LS1012A Platform
Use case in page 5 in Porting OpenWrt/LEDE on QorIQ Layerscape ARMv8 Platforms
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------