PFE not found in LSDK19.09 linux 5.4 and 5.2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PFE not found in LSDK19.09 linux 5.4 and 5.2

2,093件の閲覧回数
kai_wu
Contributor III

Hi,

I am working with LSDK 1909, and build the Linux 5.2 and Linux 5.4. I built them successfully with help from yipingwang in another question LSDK19.09 for linux 5.4 .     

But I found there is not pfe driver in both LSDK Linux 5.2 and Linux 5.4.

So I cannot see eth0 and eth1 in ls1012ardb. Is there any problem with pfe driver?  Or where I can get the pfe driver for LSDK Linux branch 5.x.         

 

Best regards,

Kai Wu

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,926件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Kai Wu ,

I upload Linux 5.4 source code downloaded from our internal git tree to you, please download it from the following link.

https://drive.google.com/open?id=1gEtKmLl572G9xoVYhRfD0qrYwDOd58Ot 

Please refer to PFE Linux Kernel driver in drivers/staging/fsl_ppfe/.

Thanks,

Yiping

0 件の賞賛
返信

1,751件の閲覧回数
shaunch-lin
Contributor I

Hi, 

I'm using openIL 1.11 with linux 5.4, LSDK 20.04

and I also meeting this problem, 

but I can see firmware file and driver by lsmod

Is there anything I can check ?

 

0 件の賞賛
返信