P1010RDB TFTP does not work

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

P1010RDB TFTP does not work

2,509 次查看
Dvorkin
Contributor I

Could anyone tell me how to use TFTP command in P1010RDB (in Linux, not in u-boot)?

The TFTP does not react any options that mentioned in other Linux userguides.

 

For example, the TFTP does not know -V option and all other options too. It does not execute commands get and put too.

 

root@p1010rdb:~# tftp -V
tftp: invalid option -- 'V'
BusyBox v1.17.1 (2011-07-05 11:11:50 HKT) multi-call binary.

Usage: tftp [OPTIONS] HOST [PORT]

 

标记 (1)
1 回复

1,389 次查看
zilitor
Contributor II

Setup a TFTP server on your desktop first. 

 

Then in the Linux shell, do these steps:

1. Configure the ethernet port

2. cd to desired directory

3. run: tftp -g -I <file name> <desktop address> <TFTP port>   //(this (-I) is either 'el' or 'eye')

 

That is what has worked for me on the P1010RDB. Hope it helps.