MPC8572DS uboot problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC8572DS uboot problem

2,063件の閲覧回数
dmitrshard
Contributor II

Hello!

I'm working on bareboard project for MPC8572DS board with MPC8572E processor. I have an elf file. This elf file is working through codewarrior tap. I need to launch my elf file from u-boot, but bootelf command in u-boot does not work. Where i can find u-boot with working bootelf command or what i need to launch my elf file from u-boot.

Thanks!

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,987件の閲覧回数
ufedor
NXP Employee
NXP Employee

I belive that it is required to prepare the binary image and load it to the memory base address used by the ELF.

To run the code it is possible to use U-Boot "go <address>" command.

0 件の賞賛
返信

1,987件の閲覧回数
addiyi
NXP Employee
NXP Employee

You have to recompile uboot with bootelf support (#define CONFIG_CMD_ELF). Also, check if your uboot version support this command.

Adrian

0 件の賞賛
返信