LS1043 platform "reset" can not work

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS1043 platform "reset" can not work

跳至解决方案
1,344 次查看
allan_yi
Contributor I

we use LS1043,it is unusefull when i input the command "reset" in uboot mode or "reboot" under the system,what should i do?

0 项奖励
回复
1 解答
1,291 次查看
ufedor
NXP Employee
NXP Employee

Ensure that RESET_REQ_B is properly connected, so that its assertion will generate PORESET_B low pulse having at least 1 ms duration.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,292 次查看
ufedor
NXP Employee
NXP Employee

Ensure that RESET_REQ_B is properly connected, so that its assertion will generate PORESET_B low pulse having at least 1 ms duration.

0 项奖励
回复
1,291 次查看
allan_yi
Contributor I

Thanks a lot ,the problem had been solved,the PORESET_B  low plus only 200ns duration befor.

0 项奖励
回复