Is "APU Unavailable Interrupt" (IVOR9) supported on e6500?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is "APU Unavailable Interrupt" (IVOR9) supported on e6500?

ソリューションへジャンプ
396件の閲覧回数
bklucz
Contributor I

The e6500 RM lists IVOR9 ("APU Unavailable") as supported register, but there is nothing in the documentation about "APU Unavailable" interrupt itself. E500 core documentation clearly states that IVOR9 is not supported, but there is no such statement in e5500/e6500 manuals.

Is the "APU Unavailable" Interrupt supported on e6500 core?
Is the IVOR9 register really supported on e6500 core?

タグ(1)
0 件の賞賛
返信
1 解決策
359件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Is the "APU Unavailable" Interrupt supported on e6500 core? yes

 

Is the IVOR9 register really supported on e6500 core? yes

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
360件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Is the "APU Unavailable" Interrupt supported on e6500 core? yes

 

Is the IVOR9 register really supported on e6500 core? yes

0 件の賞賛
返信
376件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Confirming with the AE team.

0 件の賞賛
返信