Is "APU Unavailable Interrupt" (IVOR9) supported on e6500?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is "APU Unavailable Interrupt" (IVOR9) supported on e6500?

Jump to solution
178 Views
bklucz
Contributor I

The e6500 RM lists IVOR9 ("APU Unavailable") as supported register, but there is nothing in the documentation about "APU Unavailable" interrupt itself. E500 core documentation clearly states that IVOR9 is not supported, but there is no such statement in e5500/e6500 manuals.

Is the "APU Unavailable" Interrupt supported on e6500 core?
Is the IVOR9 register really supported on e6500 core?

Tags (1)
0 Kudos
Reply
1 Solution
141 Views
yipingwang
NXP TechSupport
NXP TechSupport

Is the "APU Unavailable" Interrupt supported on e6500 core? yes

 

Is the IVOR9 register really supported on e6500 core? yes

View solution in original post

0 Kudos
Reply
2 Replies
142 Views
yipingwang
NXP TechSupport
NXP TechSupport

Is the "APU Unavailable" Interrupt supported on e6500 core? yes

 

Is the IVOR9 register really supported on e6500 core? yes

0 Kudos
Reply
158 Views
yipingwang
NXP TechSupport
NXP TechSupport

Confirming with the AE team.

0 Kudos
Reply