Is "APU Unavailable Interrupt" (IVOR9) supported on e6500?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is "APU Unavailable Interrupt" (IVOR9) supported on e6500?

跳至解决方案
179 次查看
bklucz
Contributor I

The e6500 RM lists IVOR9 ("APU Unavailable") as supported register, but there is nothing in the documentation about "APU Unavailable" interrupt itself. E500 core documentation clearly states that IVOR9 is not supported, but there is no such statement in e5500/e6500 manuals.

Is the "APU Unavailable" Interrupt supported on e6500 core?
Is the IVOR9 register really supported on e6500 core?

标记 (1)
0 项奖励
回复
1 解答
142 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Is the "APU Unavailable" Interrupt supported on e6500 core? yes

 

Is the IVOR9 register really supported on e6500 core? yes

在原帖中查看解决方案

0 项奖励
回复
2 回复数
143 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Is the "APU Unavailable" Interrupt supported on e6500 core? yes

 

Is the IVOR9 register really supported on e6500 core? yes

0 项奖励
回复
159 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Confirming with the AE team.

0 项奖励
回复